MODBUS.ERRORS

Description

Lists the last twenty Modbus errors. Each entry contains the Modbus address that was accessed and the error code of the failed Modbus request.

If more than twenty errors occur, the oldest error is dropped, and the new error is stored at the end of this list. All Modbus errors are stored regardless of the state of the error mode (MODBUS.ERRORMODE).

-->MODBUS.ERRORS
(39d:21h:30m:48s) Write 40002: Modbus error code 34 (Command Error), Error 7 (Command is read-only)
(39d:21h:45m:22s) Read 45001: Modbus error code 38 (Length Invalid) -->

Context

For more information, see Modbus Errors.

Versions

Action Version Notes

Implemented

02-05-00-000

 

General Information

Type

Info Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

See Also

MODBUS.CLRERRORS

MODBUS.ERRORCOUNT

MODBUS.ERRORMODE

Stored in Non-Volatile Memory

No